AnsweredAssumed Answered

sweep, bandwith and video resolution, span. calibrated measurament.

Question asked by thecarver on Jul 13, 2012
Latest reply on Jul 23, 2012 by tabbott
Hi,

I would want to know which is the criteria that the 8590L series spectrum analyzers have to get not uncalibrated measurament which these parameters involved. I have read the manuals but I didn't get the answer. Surfing the web I found one criteria of HP analyzers:
minimu sweep=sw; sp=span; video resolution=vb; bandwith resolution=bw;

when vb is bigger or equal than bw:

sw=2,5*(sp)/(bw^2);

if not

sw=2,5*(sp)/(bw*vb);

but, it didn't work for 8590L series. Obviusly all these parameters are set to manual in my configuration. Any of yu could help me?

Thanks in advance.  

Outcomes