AnsweredAssumed Answered

Voltage readings

Question asked by Easting on May 27, 2011
Latest reply on Jun 7, 2011 by lhornburg
I have a HP 34970A that I use to test cells and batteries during charge/discharge cycles. I want to use it to measure the voltage before cycling. Is there an easy way to configure it so that I can just connect a battery and push a button, and it automatically places the measured voltage in an Excel sheet? I don't want a reading over time, just an instantaneous voltage. I don't want to use the timer and try to keep up with its scans.

I use a scale that works great with Excel using Winwedge. Winwedge even advances to the next cell after a reading. That would be even better. Any advice welcome, thanks.  

Outcomes