AnsweredAssumed Answered

agilent 34980A clock signal and synced signals

Question asked by svt4cobra6 on May 9, 2011
Latest reply on May 10, 2011 by svt4cobra6
Just wondering if anyone is familair with the 34980A I/O card as well as the 34980A switch and measurement unit?  I need to create a delayed clock and a few delayed pulses from a master clock.  I do need precise timing on these delays,
I am wondering if it is possible to create these signals from the card, also probably could not do it with multiple writes because of the delay from the operating system,  I also have 4 of these cards.  I have a PC running HPVEE connected to the 34980A via Eithernet.
Thanks.  

Outcomes