AnsweredAssumed Answered

33500 Series Waveform Generator Creating an IQ Modulated Waveform in MATLAB

Question asked by lhornburg Employee on Oct 24, 2012
33500 Series Waveform Generator Creating an IQ Modulated Waveform in MATLAB and Generating it.

33500 Series Waveform Generator creating an IQ modulated waveform in MATLAB and generating the signal. It is easy to create an IQ waveform in MATLAB Simulink then save it as a dat file on a USB stick. The function generator can directly load the arb and then play it - with the optional IQ player.
Video:http://www.youtube.com/watch?v=qsP17Gs_7Vc

For more information:
http://www.agilent.com/find/33500b
http://www.agilent.com/find/33509b
http://www.agilent.com/find/33519b
http://www.agilent.com/find/33521b
http://www.agilent.com/find/33522b  

Outcomes