AnsweredAssumed Answered

Using Network Analyser ( N5230A) as Function Generator

Question asked by ali87 on Nov 12, 2012
Latest reply on Nov 13, 2012 by daras
Dear members, 

I would like to kindly ask you a question about the Network Analyser N5230A. Is it possible to use N5230A to generate a pure sinusoid ? In other words, can I use the spectrum analyzer, for example, as function generator to generate LO signal at 10 GHz. 

When I connect the network analyzer to the spectrum analyzer, I see a DSB signal, but I don't want the two side bands to appear with the signal. 

I appreciate your help 

Regards,

Ali  

Outcomes