Hi I have two 33522A's and have to have their sample rates of the ARB signals linked somehow so that when I change the sample rate on first one I want the second one to follow and output the wave with new rate. Is it possible to do? thanks
If you press the channel 1, or channel 2 button. Then go into the dual channel menu. There should be a menu for Rate Coupling and you can set a ratio for channel 1 to channel 2. Now when you make changes to one channel, the other channel will change as well.
I may have misunderstood your question, I was just referencing channel to channel sample rates on 1 box. Are you wanting to do this with multiple boxes?
If you press the channel 1, or channel 2 button. Then go into the dual channel menu. There should be a menu for Rate Coupling and you can set a ratio for channel 1 to channel 2. Now when you make changes to one channel, the other channel will change as well.