AnsweredAssumed Answered

53230A continuous, gap free frequency measurement

Question asked by imrehg on Jul 1, 2011
Latest reply on Nov 30, 2017 by phill
Hi,

I can't seem to figure out configure the 53230A for gap-free, continuous, ongoing measurement. Either I have to use "READ?" in a loop, which has a ~300ms gap, or have to specify a sample number (which is finite). Is there a command for setting the counter for infinite measurement (with a given gating time) and use R? or DATA:REM? to get transfer the values to the computer?  

Outcomes