AnsweredAssumed Answered

3458A SETACV SYNC

Question asked by sidney.higuchi on Jan 18, 2012
Latest reply on Oct 30, 2012 by sidney.higuchi
3458A S/N US28031584.  I'VE SELECTED ACV, SETACV SYNC, LF FILTER ON, RES .002.  I'M USING THE 3458A  TO ADJUST A PRECISION VOLTAGE SOURCE. THE 60Hz SOURCE OUTPUT IS GOING FROM STANDBY TO OPERATE AT 150Vrms; BACK TO STANDBY; TO OPERATE AT 750Vrms.  THIS SEQUENCE IS REPEATED TO ADJUST THE SOURCE RANGE.  THE PROBLEM I'M HAVING IS THAT THE 3458A ISN'T TRIGGERING TO GENERATE THE SMPL LIGHT.  I'VE WAITED FOR 2 TO 5 MINUTES WITH NO SMPL LIGHT.  WHEN I QUERY ERR, I GET ERR 102 ,ERR 104, AND 0 ERR, THEN THE 3458A STARTS TRIGGERING.   HOW LONG SHOULD A MEASUREMENT TAKE?  

Outcomes