I have a requirement for a pulse generator with an output of 5 volts 500mA and I have a 33120A available to me. Will this work? I can't find anything in the specs about current output.
I think the N6700 might be a better solution here for the 0.5A current requirement. If this is a bench application, perhaps an N6705B power analyzer with an N6751A module will be a good choice. If it is an ATE application, then I would recommend an N6700B mainframe with an N6751A module. There is a LIST function which enables the N6700 platform to create built-in and arbitrary waveforms. Let me know if you have any questions.
http://www.home.agilent.com/agilent/editorial.jspx?cc=US&lc=eng&ckey=1000001226:epsg:faq&nid=-536902324.536881979&id=1000001226:epsg:faq