No, we have an Agilent-issue PC controller for actually running the testhead, we will only be using the PC's with 64 bit Windows 7 for software development. Is there a way we can get involved in the beta testing for 08.30 or will it be released soon?
i have been suffered by a problem since i want to install a version of i3070 7.20p on thinkpad T430 notebook, win7 ,64bit, i installed an virtual PC on win7 operating system, then with Windows xp mode to install the setup software i3070 7.20p, but i am failed to install it,it shows ''Error Installing NutcRACKKER Operating Enviroment',then click OK, it shows "20000006 The OE installer process did not return success to nutinsInstallOe". and when click OK, it will continue to install till completed. but after installed you can find nothing in the folder of boards. and also can not find XVision in the right bottom corner. so can you kindly tell me how to fix the problem, we have i3070 platform in our company, we just install it to develop test software. can you give me some solution to fix this or i can directly install with win7 system? my e-mail address is :iamkenhuang@gmail.com
08.21p only supports 32 bit windows 7, all new system do ship with this version on
08.30 release will support 64 bit windows 7, but this is assumed that majority requiremnet will be for test development on PC.
do you envisage need to run testhead also at 64 bit release ?