Can anyone tell me what "err" means (other than the obvious!). I get it when either turning on HP3458A or when doing a "test" function from the front panel. The "err" message appears when it finishes doing ROM and RAM tests and when it starts the "test".
I have two 3458A's one says "self test failed" when it gives up; the other fails to a "VDC" state.
If it is beyond the user to fix can you tell me where I need to send them to get fixed, please.
Thanks
Attachments
202 hardware failure test AC board
and fails to V DC
Thanks
Unfortunately this means there is probably an issue with A2 board, which is the AC converter assembly. I would suggest sending it in to an Agilent service center for repair. The USA contact number is
toll-free:
+1 800 829-4444 Press #, then 3