AnsweredAssumed Answered

E5071C applications

Question asked by thomas9003 on Nov 6, 2012
Latest reply on Nov 12, 2012 by Dr_joel
Hi,

I'm using E5071C, 2-port Test Set, 9 kHz to 6.5 GHz without Bias Tees with the following options.

Frequency offset mode
High stability timebase
Enhanced Time Domain Analysis

My questions. 

1.What is the additional equipment needed for doing 1dB Compression point measurements with the above configuration?
 
2.Power sweep functionality with the above configuration , is it possible?
 
3.Mixer measurements, what additional options I need? 

4.IP3 Measurements, what additional options I need?

Hope you can help.

Thanks.  

Outcomes