When I do a Control-F for the "Find" function, VEE9.0 opens the search window but the "Search in:" text box is disabled. I would like to be able to change the scope of search to the entire program instead of the current function module. How do I change this default behavior in VEE9.0? In order to be able to perform a search where the scope is the entire program I have to use the mouse and access the menu path "Edit->Find" in order to obtain a search box with "Search in:" set to "Entire Program". Or from the keyboard do a "Alt-E-F".
...
*Short Cuts*
Press Ctrl+F to open the Find dialog box.
To limit the scope automatically, open Find from the Program Explorer by clicking with the right mouse button on a particular context, such as a UserFunction or UserObject.
...
I wonder this is the only way to limit a scope at the moment.
-mk