AnsweredAssumed Answered

Need advice 81101A to 33220A Setup

Question asked by sleeds on Mar 7, 2011
Latest reply on Mar 10, 2011 by lhornburg
Currently I have a procedure were it lists the Agilent 81101A to use, the steps are:
Adjust for 2 Continuous Double Pulses
Frequency: 100 Hz
Dbl Delay: 8.2 µs
Leading Edge rise: 5 ns
Amplitude: +4V HI / 0V Low
Input Impedance: 50 Ohm / 1K In

Question:
Which of the 33220A, 33521, 33522 devices can perform these steps (2 Continuous Double Pulses and Dbl Delay specifically)?

I've read through the user guides and can't seem to grasp were it can perform these.

Thanks,
Stan  

Outcomes