AnsweredAssumed Answered

phase locking two 33210A at different frequencies

Question asked by maryam on Jan 12, 2011
Latest reply on Jan 12, 2011 by stephen_mueller
I am trying to synchronize two 33210A's with 001 option at different frequencies (with square waves) .
One is at f1= 100 kHz and the other at f2 = 100kHz + 10Hz.
I tried both methods (continuous and burst mode) but have not been successful. I cannot get both waveforms to be triggered at the same time.
Is there a condition on the two frequencies for phase locking? I can easily lock if f2 is an integer multiple of f1.  

Outcomes