AnsweredAssumed Answered

RFID Burst Index Macros

Question asked by sditlevs on Jul 18, 2007
Latest reply on Jun 10, 2010 by tabbott
The RFID specific demodulation in the 89600 VSA provides a burst index feature which numbers each of the identified bursts in the signal. By selecting the Time tab in the Demodulation Properties, this index value can be changed, and the burst characteristics are reported in tabular form. However, this navigation can become tedious with repeated use.  Two macros have been created which increase or decrease the current burst index number, creating tool bar function to change the index number directly.  The attached zip file gives instruction on how to use the macros, as well as how to write your own macros.  

Attachments

Outcomes