> -----Original Message-----
> From: NEBENDAHL,BERND (A-Germany,ex1)
> Sent: Thursday, January 03, 2008 16:58
> To: 'James Haas'
> Subject: RE: [vrf] strip chart with absolute time as x-axis
>
> Hello Jim,
>
> I do have the most recent version of VEE (8.5) but the strip chart
> does not allow to my knowledge a variable spacing of the x-values and
> in addition it does not allow to set an absolute value for the first
> point (or I have seriously missed something). I would like to have the
> absolute time (HH:MM:SS format) on the x-axis, which is no problem for
> the XY-Chart for example. You can set this format for the strip chart
> as well, but this does for the above reason not help.
>
> Anyway thanks for your answer.
>
> Bernd
>
>
> > There is a strip chart display in VEE in at least version
> 8.0 (that's
> > the version I use) and perhaps some earlier versions as well.
> >
> > Jim Haas
> > Director of Engineering Services
> > Sierra Microwave Technology
> > Phone: 512-869-5007 x134
> > Fax: 512-819-9658
> > james_haas@sierramicrowave.com
> >
> >
> > -----Original Message-----
> > From: NEBENDAHL,BERND (A-Germany,ex1)
> > [mailto:bernd_nebendahl@agilent.com]
> > Sent: Thursday, January 03, 2008 8:15 AM
> > To: VRF
> > Subject: [vrf] strip chart with absolute time as x-axis
> >
> > Hello all,
> >
> > I would like to create a strip chart for data aquired at times with
> > varrying intervalls between the aquisitions (real time
> readings from a
> > DMM). I do have a solution that updates a usual YX-chart on
> a regular
> > basis and cuts out the approriate piece for the strip chart from a
> > larger array where the data are first placed when aquired from the
> > DMM.
> > However there is an ugly display flicker that makes the whole thing
> > look pretty bad.
> >
> > Any ideas?
> >
> > Thanks in advance
> >
> > Bernd
> >
> >
> > ---
> > You are currently subscribed to vrf as:
> > james_haas@sierramicrowave.com To subscribe please send an
> email to:
> > "vrf-request@lists.it.agilent.com"
> > with the word subscribe in the message body.
> > To unsubscribe send a blank email to
> > "leave-vrf@it.lists.it.agilent.com".
> > To send messages to this mailing list, email "vrf@agilent.com".
> > If you need help with the mailing list send a message to
> > "owner-vrf@it.lists.it.agilent.com".
> > Search the "unofficial vrf archive" at
> > "http://www.vrfarchive.com/vrf_archive".
> > Search the Agilent vrf archive at
> > "http://vee.engineering.agilent.com".
> >
> >
> >
> >
> >
---
You are currently subscribed to vrf as: ming_meng@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".