AnsweredAssumed Answered

AW: vrf TIMER/CLOCK???

Question asked by VRFuser on Aug 6, 2007
A USB -GPS mouse do cost around 100 Dollar maximum, and VEE software for this is available. So this is a good idea to get the time. Your problem then is - that  you have to have a GPS signal - and is this available in your insdustry environment , perhaps in a Hall ?

________________________________

Von: yarien@eu.eccosorb.com [mailto:yarien@eu.eccosorb.com]
Gesendet: Montag, 6. August 2007 07:47
An: VRF
Betreff: Re: [vrf] TIMER/CLOCK???



For the PC side have a look at license protector. You will see that they
have included some items to prevent and to trace changes on the clock of
the PC.
I am not sure how to use license protector whit vee
Friendly regards,

Yoeri Arien
Microwave engineer

EMERSON & CUMING MICROWAVE PRODUCTS N.V.
Nijverheidsstraat 7A, B-2260 Westerlo
Tel  :  +32-14-56.25.47
Fax :  +32-14-56.25.07
E-mail : yarien@eu.eccosorb.com





fukui.yutaka@jp.fujitsu.com

06/08/2007 03:39
Please respond to
fukui.yutaka@jp.fujitsu.com


To
     VRF <vrf@agilent.com>
cc
     
Subject
     Re: [vrf] TIMER/CLOCK???

     




Hi,


On the PC SW side, I do not like to change the PC's clock
in order to extend the license because this illegal walkaround
may cause some disadvantages for me.


Regards,
FUKUI Yutaka


----- Original Message -----
>From: "Gonzalo Urday" <gurday@negenex.com>
>To: VRF <vrf@agilent.com>
>Subject: [vrf] TIMER/CLOCK???
>Date: Sun, 5 Aug 2007 20:05:03 -0400
>
>
>Hello all...
>
>We control a piece of external HW that we need to upgrade, I did all
the
>initial code and it was done in VEE and I intend to continue using VEE
for
>this project..one of the new requirements is the idea of a time based
>license, (HW/SW features enabled during either as a a trial periods or
as a
>monthly subscription fee that obviously gets turned off when the user
does
>not pay or when the trial period expires)....one of the problems faced
is
>that the HW does not have a means of having an internal clock to
provide
>data or time...the HW is being redesigned to this capability but the
>question is how does one acquire time and data information from a
>reliable/authentic/independent source?? We have thought of adding a GPS
>module but pricing for this particular application is prohibitive and
even
>if we do it I have the feeling that this would require a major redesing
of
>the HW and SW to support a GPS module, the other option is to connect
to the
>internet and acquire the data from a designated web site...the problem
is
>that this a hand held and we can't force the customer to connect to the
web
>everytime the user turns on the device??? On the PC SW side we have the
same
>problem??? If the PC is not connected to the web then we have to be
forced
>to use the internal clock...but this could be manipulated by the user
to
>extend forever the license??? Does anybody have faced the same
problem???
>Any suggestions???
>
>Regards
>
>Gonzalo
>
>

Der Inhalt dieser E-Mail (inkl. aller Anlagen) ist vertraulich und ausschließlich für den Adressaten bestimmt. Jede Art der Verbreitung, Nutzung oder Vervielfältigung ist untersagt. Sollten Sie diese E-Mail irrtümlich erhalten haben, informieren Sie bitte sofort den Absender und löschen die E-Mail.

Unternehmensangaben der Gesellschaften mit Sitz in Deutschland:

Pilkington Holding GmbH, Haydnstraße 19, 45884 Gelsenkirchen
Sitz: Gelsenkirchen, Amtsgericht Gelsenkirchen HRB 8997 
Geschäftsführung: Jochen Settelmayer (Vorsitz), Dr. Clemens Miller, Thomas Kretschmann, Robert Hales
Vorsitzender des Aufsichtsrates: Dr. Axel Wiesener

Pilkington Deutschland AG, Haydnstraße 19, 45884 Gelsenkirchen         
Sitz: Gelsenkirchen, Amtsgericht Gelsenkirchen HRB 2707
Vorstand: Dr. Clemens Miller, Jochen Settelmayer
Vorsitzender des Aufsichtsrates: Dr. Axel Wiesener

Pilkington Automotive Deutschland GmbH, Otto-Seeling-Straße 7, 58455 Witten
Sitz: Witten, Amtsgericht Bochum HRB 8443
Geschäftsführung: Thomas Kretschmann
Vorsitzender des Aufsichtsrates: Jochen Settelmayer

Bauglasindustrie GmbH, Hüttenstraße 33, 66839 Schmelz / Saar
Sitz: Schmelz / Saar, Amtsgericht Saarbrücken HRB 52020
Geschäftsführung: Manfred Ebbers


---
You are currently subscribed to vrf as: hua_jing@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes