AnsweredAssumed Answered

11729C option H33 carrier noise test set

Question asked by jfphp on Jan 29, 2011
Latest reply on Mar 7, 2011 by RayH
I am looking for some informations about the option H33 of the 11729C carrier noise test set : it is obviously for performing phase noise mesurements in the mm range but what kind of downconverter is used, is there a software implementation in the normal 3048A software... ? According to the HP catalog 1992 there is an application note 385 "Millimeter mesurements using the HP3048A phase noise mesurement system" (P/N 5951-6749). Can I get a copy ? Thanks.  

Outcomes