AnsweredAssumed Answered

vrf vrf - IEEE command for PNA - Marker Delay?

Question asked by VRFuser on May 12, 2008

I found it using the handy-dandy "Home/Programming" in PNA help where it has:



Programming Guide



  _____  



Two ways to find programming commands:



1.

From a simulated PNA User Interface

New

mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/XComFinderSet.htm

Legacy

mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/CommandFinderSet.htm



 



 

GPIB / SCPI

COM

2.

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/GP-IB_Command_Finder/SCPI_Command_Tree.htm"Command Tree

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/COM_Reference/Objects/The_Analyzer_Object_Model.htm"COM Object Model

See Also

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/GPIB_Example_Programs/SCPI_Example_Programs.htm"Example Programs

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/COM_Example_Programs/COM_Example_Intro.htm"Example Programs

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/Learning_about_GPIB/Learning_about_GPIB.htm"Learning about GPIB

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/Learning_about_COM/Learning_about_COM.htm"Learning about COM


 
And I use the "From a Simulated PNA user interface" to find the commands related to a pulldown, which are:
 

CALCulate<cnum>:MARKer<mkr>:SET <char> 


(Write-only) Sets the selected instrument setting to assume the value of the specified marker.

Marker Functions CENT, SPAN, STARt, and STOP do not work with channels that are in HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/S1_Settings/Sweep.htm#SweepTypeDiag"CW or HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/S1_Settings/Sweep.htm#segment"Segment Sweep mode.

HYPERLINK "mk:@MSITStore:C:dataWorkPNAHelpFilespnahelp8_0.chm::/Programming/GP-IB_Command_Finder/Calculate/Marker.htm#Critical"See Critical Note

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<mkr>

Any marker number from 1 to 10; if unspecified, value is set to 1

<char>

Choose from:

CENTer - changes center frequency to the value of the marker

SPAN -  changes the sweep span to the span that is defined by the delta marker and the marker that it references. Unavailable if there is no delta marker.

STARt - changes the start frequency to the value of the marker

STOP - changes the stop frequency to the value of the marker

RLEVel - changes the reference level to the value of the marker

DELay - changes the line length at the receiver input to the phase slope at the active marker stimulus position.

Examples

CALC:MARK:SET CENT
calculate2:marker8:set span

Query Syntax

Not Applicable

HYPERLINK "javascript&#058;hhctrl.TextPopup(DefSCPI,'Arial,8',10,10,00000000,0xc0ffff)"Default

Not Applicable

 

 

  _____  


  _____  

From: Walker, Richard [mailto:Richard.Walker@Herley.Com]
Sent: Monday, May 12, 2008 8:41 AM
To: PDL-LISTS,VRF (A-Lists,unix1)
Subject: [vrf] vrf - IEEE command for PNA - Marker > Delay?



Vee users,

            Can someone point me in the correct direction for the IEEE command (Marker to Delay)?

 

Thanks

 

Richard A. Walker

RF Automation Specialist, LLC

Cell: (631) 834-6293

 


  _____  

The information contained in this message may be confidential and legally privileged. If you are not the intended recipient of this email and its attachments, you must take no action based upon them, nor must you copy or show them to anyone.
Please contact the sender if you believe you have received this email in error.







---
You are currently subscribed to vrf as: joel_dunsmore@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".


---
You are currently subscribed to vrf as: ming_meng@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".  

Outcomes