Hi Vrf,
I have a machine with VeePro 7.5 & IO lib 14 installed running XP Pro.
I have recently upgraded to VeePro 8.
The problem that I have is that when I try to Install IO lib 14.2 it tells me to uninstall 14.0
If I go to Add/Remove programs in the Control program IO 14 is not listed.
Anybody got any idea how I can Uninstall IO Lib14?
So that I can Install 14.2.
Any advice would be appreciated.
Best Regards
Gavin.
--- You are currently subscribed to vrf as: hua_jing@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body. To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com". To send messages to this mailing list, email "vrf@agilent.com". If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com". Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive". Search the Agilent vrf archive at "http://vee.engineering.agilent.com".