Hi All,
I need to programmatically (via SCPI) assign Channel B of a E4417A power meter to Recorder output #1. When I send the OUTP:REC1:STAT ON command, the unit assigns Channel A to recorder output #1 and if I send OUTP:REC2:STAT ON, the unit assigns Channel B to recorder output #2.
I've gone through the programming manual and have tried the OUTP:REC1:FEED CALC2 method but this does not work and no other command seems to come close to providing the feature I need.
From the front panel, it is quite simple to manually assign Channel B to Recorder output 1 but for some reason, I'm stumped when trying to do this via SCPI commands. The fact that the unit reads the numbers 1 for A and 2 for B in its programming commands, also contributes to some confusion!
Any help would be greatly appreciated!
Thanks!
John
I need to programmatically (via SCPI) assign Channel B of a E4417A power meter to Recorder output #1. When I send the OUTP:REC1:STAT ON command, the unit assigns Channel A to recorder output #1 and if I send OUTP:REC2:STAT ON, the unit assigns Channel B to recorder output #2.
I've gone through the programming manual and have tried the OUTP:REC1:FEED CALC2 method but this does not work and no other command seems to come close to providing the feature I need.
From the front panel, it is quite simple to manually assign Channel B to Recorder output 1 but for some reason, I'm stumped when trying to do this via SCPI commands. The fact that the unit reads the numbers 1 for A and 2 for B in its programming commands, also contributes to some confusion!
Any help would be greatly appreciated!
Thanks!
John