AnsweredAssumed Answered

AW: vrf Matlab Skript doesn't start

Question asked by a.kieser on Nov 4, 2007
Thanks for the answer,
but it's quite stupid to change the path and the COM-server registration everytime I use matlab or Vee...
 
Are there any other ideas?
 
If not, I think it can be done with a batch-routine, but I have no idea to remove one - and only one directory from the PATH-Variable... Any idea for this?
 
Thanks in advance, Axel
 

  _____  

Von: Boespflug, Matthew (GE, Research) [mailto:boespflu@research.ge.com]
Gesendet: Freitag, 2. November 2007 18:10
An: VRF
Betreff: RE: [vrf] Matlab Skript doesn't start


Axel,
 
I have run into a similar problem. Cao Luo (Agilent) helped solve the issue (Thanks Cao). The following two emails might be able to help:
1)

Hi Matthew,

Do you install a standalone MATLAB on your machine?

I met the similar case once: a standalone MATLAB is installed on the PC and VEE Pro uses the standalone MATLAB to run the MATLAB script; the standalone MATLAB uses network license, so if the PC doesn’t connect to the network, the standalone MATLAB will fail at the startup and VEE Pro will report this error.

2)

Matt,

It is true that VEE can use own built-in MATLAB engine. 

VEE uses MATLAB engine through MATLAB COM server.  But there can only be one MATLAB COM server on the PC. After VEE installs, VEE will register the built-in MATLAB engine as the COM server at the first run if there is no MATLAB COM server exists. But when you install a standalone MATLAB on your PC, the standalone MATLAB will register its self as the MATLAB COM server, which is why VEE will choose the standalone MATLAB to run the MATLAB script.

If you want to use the built-in MATLAB engine to run the MATLAB script in VEE, you can do this: go to <VEE install dir>matlab inwin32 in command line, run command “matlab /regserver”, which will register the built-in MATLAB engine in VEE as COM server; after that you need to remove the path of the standalone MATLAB installation dir from the system variable “Path”, which may impact the usage of the standalone MATLAB. 

If you want to use the standalone MATLAB to run the MATLAB script in VEE, you need to register the standalone MATLAB as the COM server, the command is still “matlab /regserver”, and also the path of the standalone MATLAB installation dir should be added back to the system variable “Path”. 

Hope this will help.

Cao Luo.

Matthew Boespflug
GE Global Research
1 Research Circle
ES - 508c
Niskayuna, NY 12309

Phone: 518-387-5017
Fax: 518-387-7989
boespflu@research.ge.com
GE Company Proprietary Information
www.geglobalresearch.com


 

  _____  

From: a.kieser@francotyp.com [mailto:a.kieser@francotyp.com]
Sent: Friday, November 02, 2007 9:56 AM
To: VRF
Subject: [vrf] Matlab Skript doesn't start



Hi there,
after installing matlab R2006b I can't start any matlab-Skripts within VEE 7.51, because there is always the error (I don't know the correct english sentence…) 'Prozedureinsprungpunkt "utCsqrt" was not found in DLL "libut.dll".

After googleing I found out that this is because of a wrong version between different applications using matlab and has sth. to do with the path variable.

But what can I do??

Any Hints?

Greetings, Axel.


**********************************************************************

"LEGAL DISCLAIMER: As you are aware, messages sent by eMail can be manipulated or diverted by third parties. If not mentioned otherwise our eMail messages are generally not legally binding. This electronic message (including any attachments) contains confidential information and may be legally privileged or otherwise protected from disclosure and as such is intended only for the use by the intended recipients. Please be aware that any unauthorized disclosure, copy, distribution or use of the contents of this message is expressly prohibited. If you have received this eMail in error please understand that you must not copy this eMail or any attachment or disclose the contents to any other person. Please notify us immediately by reply eMail and delete this message and any attachments from your system. Thank you for your cooperation". The FP Group

**********************************************************************

 


---
You are currently subscribed to vrf as: boespflu@research.ge.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".
---
You are currently subscribed to vrf as: a.kieser@francotyp.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".
---
You are currently subscribed to vrf as: ming_meng@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".  

Outcomes