So i have this quick question.
My system has a Network Analyzer from Agilent. However as my system will be sent to other facilities It might happen where that facility will use a very similar Agilent analyzer but not the same mode. Is there any way to write the code and set it up where the user can connect different models and then select them from the a list. At the moment if i connect the hardware i can see it in Instrument Manager, but can i add just a blank instrument? Some ideas but not 100% sure.
Thank you
My system has a Network Analyzer from Agilent. However as my system will be sent to other facilities It might happen where that facility will use a very similar Agilent analyzer but not the same mode. Is there any way to write the code and set it up where the user can connect different models and then select them from the a list. At the moment if i connect the hardware i can see it in Instrument Manager, but can i add just a blank instrument? Some ideas but not 100% sure.
Thank you
Then in Connection Expert, you can set up each different models with a specific Alias.
Then using the instrument block in VEE, you can assign Alias to the block depending on the selection of the model. Then the block will communicate/belongs to the instrument with the same alias that you assigned.
Make sense?