AnsweredAssumed Answered

vrf UserObjects that are panels.

Question asked by soeren.hedemand on Aug 17, 2007
Hi Marcus.
 
This is very interesting! It is a Vee 8 feature, right?
 
/Søren

  _____  

From: Engelke Marcus (Nokia-M/Bochum)
Sent: 2007-08-16 16:25
To: VRF
Cc: Hedemand Soeren (Nokia-MP/Copenhagen)
Subject: RE: [vrf] UserObjects that are panels.


Hi,
 
 in fact you need a function with a panel to show userobject panels...but to have it dynamically (if this is your intention)...check out the attached demo and press the buttons in the main while watching the fct panel

Yours sincerely,
  Marcus 



  _____  

From: ext bounce-5388997-5352538@it.lists.it.agilent.com [mailto:bounce-5388997-5352538@it.lists.it.agilent.com]
Sent: Donnerstag, 16. August 2007 15:44
To: VRF
Subject: [vrf] UserObjects that are panels.



Hi all.

It is possible in Vee to turn a userobject into a panel, without the function that the userobject exists in being a panel.

If you set showPanelOnExecute to ON, it works fine. But what if you want to show or hide such a panel from a different userfunction? How do you do that?

/Søren


---
You are currently subscribed to vrf as: marcus.engelke@nokia.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".
---
You are currently subscribed to vrf as: hua_jing@agilent.com
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list, email "vrf@agilent.com".
If you need help with the mailing list send a message to
"owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".  

Outcomes