AnsweredAssumed Answered

vrf .NET Problems

Question asked by fukui.yutaka on Aug 25, 2008
Hi,


My PC is OS:Windows XP SP3, IO Lib 15.0.11221.0.
When I try to open ".NET Assembly References" under VEE 7.03, I get the same serious error:  Internal Error : (0xE0434F4D), Error number: 999. However, it works OK under VEE7.5, VEE8.0 and VEE8.5 on the same PC.


Regards,
FUKUI Yutaka


----- Original Message -----
>Subject: [vrf] .NET Problems
>Date: Mon, 25 Aug 2008 09:23:11 +0200
>From: Kr?ger, Bernd <bkrueger@pil.de>
>To: VRF <vrf@agilent.com>
>
>
>Hello All,
>I am using a xxx.dll with .NET on three PC's. First everything was OK
>on one
PC. Now I have trouble when calling Devices/ .NET Assembly... Then I get a ser ious error:  Internal Error : (0xE0434F4D), Error number: 999. This PC is a P4  2,4GHz, Windows 2k, VEE 7.03, IO Lib 15.0.10528.0. My first tries with this d ll I had a Evaluation VEE 8.5. Maybe this is the reason? Before I forget: some times I get an error too when windows starts: Agilent IO Control could not sta rt because there was a problem communicating with the Agilent IO Libraries Ser vice.
>
>
>Well. Then I tried the second PC (Win2k, VEE 5.02 and VEE 7.03, IO Lib
>14.1.8
016.0)and the same error as mentioned above came up(serious error...).
>The last try was a Notebook (Win XP, VEE 7.03, IO Lib 15.0.10528.0) and
>it wa
s OK. Next day the same error happend.
>
>After this serious error VEE works OK except this .NET things. And even
>the s
econd time I open Device/ .NET Assembly... It seems to be OK. I have to browse  for the .dll and load it. But starting the aplication another error occured:
.NET object could not be created (error 756).
>
>I am not familiar with this .NET things. This .dll symplifies some
>RS232 comm
ands to our sensors. Maybe its only several VEE's on one and the same PC?
>
>Thanks in advance
>
>Bernd
>
>
>---
>You are currently subscribed to vrf as: fukui.yutaka@jp.fujitsu.com To
>subscribe please send an email to: "vrf-request@lists.it.agilent.com"
>with
the word subscribe in the message body.
>To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
>To send messages to this mailing list,  email "vrf@agilent.com". 
>If you need help with the mailing list send a message to
>"owner-vrf@it.lists.it.agilent.com".
>Search the "unofficial vrf archive" at
>"http://www.vrfarchive.com/vrf_archive
".
>Search the Agilent vrf archive at "http://vee.engineering.agilent.com".
>

== ? =====================================================================
FUJITSU ???(?)????[?9-432] ?????????
  ?????????)??·?????????? ? ??  ? (FUKUI Yutaka) INTERNET E-Mail: fukui.yutaka@jp.fujitsu.com
TEL: 044-754-2238(ext:711-5-3153)     FAX: 044-754-2434(ext:711-5-3178)
== ? =====================================================================



---
You are currently subscribed to vrf as: hua_jing@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes