AnsweredAssumed Answered

AW: vrf Multiple VEE versions on the same PC

Question asked by VRFuser on Aug 15, 2008

Doubleclicking always opens the actual VEE version- so be warned- it saves also with for example VEE8.5 If you want to be parallel with your programs, i do recommend to put a version number in your programname.
Change your VEE.exe   V6 also to Vee6.exe for example, and you can do this parallel working automatically- in case that you get problems with the newer versions...
Hope you do understand...rename your files with the versions you want to open and store, and rename your different VEE versions also with a versionname. The only version which makes problems with this renaming was V85... Therefore it is still VEE.exe

detlef

-----Ursprüngliche Nachricht-----
Von: Stan Bischof (Richard S) [mailto:rsb@soco.agilent.com]
Gesendet: Freitag, 15. August 2008 16:16
An: VRF
Cc: vrf@agilent.com
Betreff: Re: [vrf] Multiple VEE versions on the same PC

"Dr. Hans-Joachim Fischer" <HJFischer@fischer-tech.de> wrote:
> I am still using VEE 6.2. Now I want to install VEE 7.5, as VEE 6.2
> has unresolvable internal bugs (1.VEE built-in functions do not
> execute due to missing input data - the debugger shows that input data
> are available. 2. Globally defined real variables show wrong values
> when reading it.)
>
> Is it possible to install both versions on the same PC? What about the
> runtime version for my customer. Which version(s) should he use?
>
> What about upgrading to VEE 8.5. Can I also install this version in
> parallel on the same PC as the older versions?
>

I typically have 2 or 3 versions on the same machine since I do a fair amount of support. No issues in VEE itself. The only issue that can get a little sticky is that you get exactly one IO libaries so occasionally there's compatibility issues in trying to find one IO lib that works right with all the versions of VEE.
Most of the time though using latest/greatest IO lib does the trick.

Bottom line though- no problem having multiple VEE versions.

Stan


--------------------------------------------------------------------------
Stan Bischof  Agilent Technologies  707-577-3994  stan_bischof@agilent.com
--------------------------------------------------------------------------


---
You are currently subscribed to vrf as: Detlef.Baranski@pilkington.de To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".


Der Inhalt dieser E-Mail (inkl. aller Anlagen) ist vertraulich und ausschließlich für den Adressaten bestimmt. Jede Art der Verbreitung, Nutzung oder Vervielfältigung ist untersagt. Sollten Sie diese E-Mail irrtümlich erhalten haben, informieren Sie bitte sofort den Absender und löschen die E-Mail.

Unternehmensangaben der Gesellschaften mit Sitz in Deutschland:

Pilkington Holding GmbH, Haydnstraße 19, 45884 Gelsenkirchen
Sitz: Gelsenkirchen, Amtsgericht Gelsenkirchen HRB 8997
Geschäftsführung: Dr. Clemens Miller (Vorsitz), Jochen Settelmayer, Thomas Kretschmann, Robert Hales Vorsitzender des Aufsichtsrates: Dr. Axel Wiesener

Pilkington Deutschland AG, Haydnstraße 19, 45884 Gelsenkirchen         
Sitz: Gelsenkirchen, Amtsgericht Gelsenkirchen HRB 2707
Vorstand: Dr. Clemens Miller, Jochen Settelmayer Vorsitzender des Aufsichtsrates: Dr. Axel Wiesener

Pilkington Automotive Deutschland GmbH, Otto-Seeling-Straße 7, 58455 Witten
Sitz: Witten, Amtsgericht Bochum HRB 8443
Geschäftsführung: Thomas Kretschmann
Vorsitzender des Aufsichtsrates: Jochen Settelmayer

Bauglasindustrie GmbH, Hüttenstraße 33, 66839 Schmelz / Saar
Sitz: Schmelz / Saar, Amtsgericht Saarbrücken HRB 52020
Geschäftsführung: Manfred Ebbers


---
You are currently subscribed to vrf as: hua_jing@agilent.com To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "http://www.vrfarchive.com/vrf_archive".
Search the Agilent vrf archive at "http://vee.engineering.agilent.com".

Outcomes