HI
i m using agilent 8267C PSG to generate IQ data and using HMC495 direct modulator to modulate baseband IQ signals and using VSA software 89600 to demodulate and check the signals. kindly assist me in doing settings of PSG and VSA. i have only flexible demodulation personility in VSA i.e AYA option.
regards
rajput
i m using agilent 8267C PSG to generate IQ data and using HMC495 direct modulator to modulate baseband IQ signals and using VSA software 89600 to demodulate and check the signals. kindly assist me in doing settings of PSG and VSA. i have only flexible demodulation personility in VSA i.e AYA option.
regards
rajput
To configure the 89600 VSA to use your PSG source, make sure that you have added the source using the Agilent IO Libraries Connection Expert. Then, open the 89600 VSA and click Utilities > Hardware > Source tab, clear the Simulate Hardware check box, and select the box next to the PSG that you want to use.
You can find more information about configuring sources in the 89600 VSA online help by clicking Help > Roadmap and then navigating the Table of Contents to Measurement Platforms > Measurement Hardware > Agilent Sources.
Also, once you've configured the 89600 VSA to use the PSG, you will be able to use the Source menu to configure the source. The 89600 VSA only supports configuring the source to use arbitrary waveforms (from VSA recordings) or to generate a sine wave, so you will need to use the internal PSG signal generation options or Signal Studio if you want to do more than the 89600 VSA can configure the source for.
Regards,
Caleb