AnsweredAssumed Answered

Turn Off Signal After Single-Epoch of Modulation

Question asked by RadarGuy on Dec 29, 2011
Hello,

I'm using the E4438C "Real Time I/Q Baseband Generator" to produce a QPSK signal from a user-defined file (with 1 second worth of symbols).  I configured the system to single-run and external trigger, so it only generates the 1 second modulation at the rising edge of the trigger.  The problem I have is that at the end of the 1 second modulation the system continues to transmit the final symbol, which here produces a tone. 

I need to determine a method to have the signal completely shut off after the final symbol.  Is a setting option that produces this effect?  FYI, I have available a TTL pulse that corresponds to the time I want the system to shut off.  Is there any way to use that to trigger the system to turn off the RF power?

Any help would be appreciated.

Thanks,
Steve  

Outcomes