AnsweredAssumed Answered

Data Logging in 34411A using C

Question asked by sriduttvnayak on Apr 4, 2013
Latest reply on Apr 15, 2013 by sriduttvnayak
I have written a code to do the following.
1. Initialize DMM.
2. Take x number of readings in sync with external trigger.
3. Save it to text file.

The problem is that the code doesn't return till all this is completed. That means it is blocking the execution of other code. 
(Ex: Other Hardware which generates these triggers).

I have used :
Ag34410_InitWithOptions
Ag34410_ConfigureMultiPoint
Ag34410_ConfigureTrigger
Ag34410_FetchMultiPoint

Is there a way to use the DMM-session in such a way that it returns back the control after session is initialized and started so that other hardware or operations can be started.

The attached code has the changes I have done using the Example code.  

Attachments

Outcomes