AnsweredAssumed Answered

33522A - Synching both channels

Question asked by rcoolbaugh on Nov 2, 2011
Latest reply on Nov 7, 2011 by lhornburg
I'm trying to get both channels to sync in the following mode :

ch 1 is running an arbitrary waveform at 1kHz
ch 2 is running a square wave at 1kHz
both channels are in gated burst mode so I can disable them with an external input

During init. when I activate both channels they don't come up in phase with one another.  Sync is on with ch1 as the source.
The PHASE:SYNC command is rejected.  Ideally I would use the sync output for the square wave but that appears to be disabled when I go into gated burst mode.

Any ideas?  

Outcomes