AnsweredAssumed Answered

Connection Expert issue (82357B to Agilent/HP 8648D/HP8562E)

Question asked by tonyku on Mar 18, 2013
Latest reply on Mar 25, 2013 by MikeM
Hi,

Have an issue with 82357B USB connection with Connection Expert.  When I connect it to these two devices, I was not able to get the ID of the machines.   The help section says that if auto-identification is turned off, then it would be OK if the machines do not support 488.2.   The specs says they support IEEE 488 (didn't indicate .2). 

Tony Ku  

Outcomes