AnsweredAssumed Answered

34980 / 34937A display, keypad vs web interface

Question asked by drdroege Employee on Sep 8, 2011
Latest reply on Sep 9, 2011 by lhornburg
I'm confused with switch setting differences that are displayed on the 34937A/34980A vs. those displayed using the web interface.

For example:
A relay setting for a channel on the 34937A is displayed on the 34980A as OPEN while the web interface display for that same relay displays NC (Normally Closed).
Likewise, if the switch is changed to CLOSED, the web interface displays the switch in the NO (Normally Open) position.

It seems as though the NC and NO positions displayed on the web interface are reversed.  What am I missing?

Thanks,
David  

Outcomes