Hello,
is it possible to synchronize two or more function generators from different series? Both devices have option 001 installed.
Thanks in Advance!
is it possible to synchronize two or more function generators from different series? Both devices have option 001 installed.
Thanks in Advance!
Yes, you can connect the 33200-series and the 33500-series together the same way you would if you were connecting two generators within the same family. Select one unit or an external reference to be the master source, and fan the connections to the other units.
We have an application note available at http://cp.literature.agilent.com/litweb/pdf/5990-3467EN.pdf
Best Regards,
Cheryl