AnsweredAssumed Answered

Multi-Carrier Power measurements

Question asked by Leyo on Aug 7, 2012
Hello,

This is regarding the power measurements of GSM based signals.

Suppose I have one GSM carrier with all 8 TS on and each slot has 10W power. Because of the guard period in GSM structure, the actual power read by the power meter will be 0.25 dB low.
So in this case power meter will read 40-0.25=39.75 dBm.
Now consider the case where TS0 has 10 W, TS1->8W, TS3->5W,TS4->3W,Ts5->10WTS6->8W,TS7->9W. In this case what will be the reading of Power meter?

Thanks,
Leyo

Outcomes