AnsweredAssumed Answered

E4413A Calibration factors

Question asked by MICROWAVE68 on Sep 13, 2008
I want to read out and the restore the calibration factors of a E4413A , i know the commands and syntax to readout the info as well as how to restore it, however im looking for some further info on the memory organization as in which memory location holds what, i know that the sensor has two ranges so i assume that there are calibration factors for both ranges as well as possibly linearity and temperature correction factors, any info would be appreciated, NDA can be signed  

Outcomes