Hi,
I am trying to run some tests on a 10/100 interface with a link partner, but I cannot establish a link through the test fixture using section 6 of the fixture. I think I have the connections correct, as there are only two Ethernet ports within section 6.
Are there any tests I can run on the test fixture itself to check to see if it is damaged? Without being able to signal through the board there is no way to establish a link with the link partner so at this point I am dead in the water.
Thanks,
Jeff
I am trying to run some tests on a 10/100 interface with a link partner, but I cannot establish a link through the test fixture using section 6 of the fixture. I think I have the connections correct, as there are only two Ethernet ports within section 6.
Are there any tests I can run on the test fixture itself to check to see if it is damaged? Without being able to signal through the board there is no way to establish a link with the link partner so at this point I am dead in the water.
Thanks,
Jeff
there is no passthru section on the fixture.