AnsweredAssumed Answered

Excel ActiveX

Question asked by VRFuser on Feb 12, 2001
Hello All,

i have a little problem with Excel activeX. On some PCs my application is
running very well, but on some the Excel activeX driver isn't running. All PCs
are in one network, and Excel is installed on the network. On the PCs, where my
application isn't running the excel (VEE )error are not the same (Errors are for
example 563 or 557) . Has anyone an idea, where i can look after?  Or any other
solutions? The vee application was written in vee 5.01.

Greetings

Ralf Eichele


---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes