AnsweredAssumed Answered

N5182A MXG remote I/Q calibration error

Question asked by cdl on Sep 16, 2011
Latest reply on Oct 25, 2011 by tabbott
When sending the direct I/O command ":CALibration:IQ:FULL" using Vee, the instrument starts its I/Q calibration. But after 2 -3 % it aborts and gives the error message: 517, Calibration failure; Cal aborted by user. However, the only command sent is the ":CALibration:IQ:FULL". The command is sent using LAN direct I/O. Other commands work fine. Any hints??  

Outcomes