Is it possible to do manual programming of the 66000A using the only the 66001A keyboard? I need to be able to bring up the power supplies in the mainframe in a certain order to avoid damaging the internal components of UUT's. i. e. turn-on subaddress 1 on first then 0, 3, 4, 2, and then turn-off in reverse order. This setup does not have any ext programming system such as a computer, just the 66001A keyboard. Using the save and recall feature, there is no guarantee of what order the power supplies turn on or off.
You may be able to do this using the list system of the 66000A which is accessible from the keyboard. What you would have to so is set up a 2 point list for each channel. The first point will be zero and the second will be whatever your final voltage is. The dwell time for the first point will essentially be your delay time. When you want to turn on, you can enable the output and then initiate and run your list.
Let me know if this works out.