AnsweredAssumed Answered

vrf data from excel

Question asked by curtis.benham on Mar 21, 2001
Hello Andrew,

     I just had this same problem.  Yes, it is possible, though
the process is a little circuitous.  Read in your array of
values... i.e.

ExcelData = Sheet.Range(Sheet.Cells(3,2), Sheet.Cells(8,6));

     Where "ExcelData" is an output pin on your formula block.  The
output pin data format is, for some reason, a record format with a
different field for element of the array.  Connect the "ExcelData"
output to a "To String" I/O transaction containing something like this:

     WRITE TEXT a REAL FIX:2 EOL

     The "To String" transaction output is connected to a
"From String" transaction containing something like this:

     READ TEXT x REAL ARRAY:6,5

     This procedure is not without it's problems however... I tried to
read
in an entire spectrum analyzer trace previously exported to Excel
[ArraySize(401,1)], and found the resultant text string to be too long for
HP VEE 5.01 to handle.  Furthermore, some of the data points miraculously
acquired 8 significant digits.  For smaller arrays, this procedure works
fine,
but funny things start happening when the array gets large.

Regards,

Curtis

-----Original Message-----
From: Muddiman, Andrew [mailto:muddimaa@tycoelectronics.com]
Sent: Wednesday, March 21, 2001 7:49 PM
To: 'vrf@lvld.agilent.com'
Subject: vrf data from excel


Hi all

Does anyone know if it is possible to bring data  from a specified area of
an excel sheet into vee as an array through the active-x medium. Also I
can't seem to get any of the paste special commands to work when takeing
them from a macro run in excel and using them in active-x with vee. Has
anyone found any code that works.

Thanks in advance

Andrew Muddiman
M/A-Com Eurotec opertations,
Loughmahon Technology Park,
Skehard Road, Blackrock
Cork ,Ireland

Phone: 00 353 21 4808372
Fax: + 353 21 4808357
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------
---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes