Hi
is there a SCPI command to increment or decrement the start and stop amplitude values on a cw freq power sweep? Using an E8257D.
thanks.
is there a SCPI command to increment or decrement the start and stop amplitude values on a cw freq power sweep? Using an E8257D.
thanks.
I would like to add either a STEP or an UP or DN command to the end of this command
[:SOURce]:POWer:STARt <val><unit>
in some way shape or form, to step the power start value up and down. Same with the
[:SOURce]:POWer:STOP <val><unit>
command. but it doesn't seem to work,. i get header error on the synth s when Itry it.