AnsweredAssumed Answered

Required option for EMI Average detector on a CXA N9000

Question asked by joro on Apr 10, 2013
Latest reply on Apr 11, 2013 by joro
Hello,

I do want to use the EMI Average detector in spectrum analyzer mode on a CXA N9000.
In the programming manual (for the command: "[:SENSe]:DETector:TRACe" ) it is stated:
               EMI Average
               Only appears with the N6141A or W6141A application or Option EMC installed and licensed.

The *IDN? response of my CXA N9000 is: "Agilent Technologies,N9000A,MYXXXXXXX,A.10.52"
The SYST:OPT response of my CXA N9000 is: "503,P03,SSD,PC3"

Based on this information I assume that the "EMC" option is not included on my CXA.  

At this moment I do have the following questions:
1) How do I know if the W6141A application is present on my CXA? (Is it always included with firmware version >= A.07.04 ?)
2) If the W6141A application is present. Can I then also use the EMI Average detector in Spectrum Analyzer trace measurements?
3) Is it possible to use the EMI Average detector in Spectrum Analyzer trace measurements?

Thanks in advance!

John  

Outcomes