AnsweredAssumed Answered

troubles using de_embeds2p symbol

Question asked by usuaria_ads on Oct 11, 2012
Latest reply on Oct 19, 2012 by eyeung
I'm trying to use a embed data file in order to negate 2-port circuit by using .s2p data file (specifically s21) but I can't obtain a right result. ¿Is there any file or desing restriction?

My design is very simple, it is composed of s2p file of a attenuator  from a PNA, but the ads simulator doesn´t carry on a right result (I main in certain frequency if s21=-60 dB I understand the right answer will be s21(embed)=60 dB but ads simulator gets 25 dB)

Could anyone explain me how I should use the embed symbol?

Thanks in advanced.  

Outcomes