AnsweredAssumed Answered

vrf Question on Saving Panels

Question asked by VRFuser on Feb 19, 2001
Dear VRF Digest

In using the SavePanelImage function to save jpeg images is there a way
to save the entire Vee screen. My applications GUI is made up of several
(10+) separate functions which are displayed using the ShowPanel
function to place them in a particular area of the screen in a certain
order. When I use the SavePanelImage you have to specify a particular
panel to save, even specifying "Execution Window" as mentioned in the
on-line help I do not get the full Vee windows as expected. Any Advice?,
am I missing something?

thanks in advance,

Steve G.

---------------------------------------------------------------------
This is the "vrf" maillist, managed by Majordomo.  To send messages to
this maillist, just email to "vrf@lvld.agilent.com".  Subscriptions and
unsubscriptions are done through the address "vrf-request@lvld.agilent.com".
If you need details, just send a message containing the text "help"
to "vrf-request@lvld.agilent.com".
---------------------------------------------------------------------

Outcomes