AnsweredAssumed Answered

Agilent 34405A firmware update problem

Question asked by Crusader on Sep 30, 2011
Latest reply on Nov 23, 2014 by krzysiekg
Hi,

we have problem using two Agilent 34405A via USB on the same computer. We have the same behaviour as stated here :

http://forums.ni.com/t5/Instrument-Cont ... -p/1037020

The serial number seem to be corrupted randmonly, and I event get a BSOD (blue screen of death) when starting one 34405A...

I've try to update the firmware to the latest one available (1.40-3.11) but without luck. Every time I get the error :

"Firmware checking condition set in engineer program is invalid (eg. wrong amout of firmware revision)."

The current firmware in the instrument is : 1.19-3.05

Is there something I can do ?

The serial number are : TW46250080 and TW46250022

Thanks you for a fast answer.  

Outcomes