AnsweredAssumed Answered

PNAX won't save Spar data / Comb reference

Question asked by lcormier on Mar 22, 2013
Latest reply on Mar 27, 2013 by lcormier
N5242A
Firmware A.09.85.06  (thanks, Dave)

Two questions.
If I have a valid Xparameter cal, enable S-parameters, then setup and take an S-measurement, I should be able to save the sparameter data, correct? I can see the s-parameter data onscreen, but " no measurement data if I try to save. I setup to save wave/Sparams, tried both .s2p and mdif.

If I put a short 3.5mm female-female thru on the comb generator at Port1 during phase reference cal, do I have to have an s2p file to represent the f-f thru? And, if so, does it effect the FB and/or XS/Xt terms?

Edited by: lcormier on Mar 22, 2013 8:49 AM

Edited by: lcormier on Mar 22, 2013 9:09 AM

Edited by: lcormier on Mar 22, 2013 9:12 AM  

Outcomes