AnsweredAssumed Answered

Benchlink - Query UNTERMINATED

Question asked by smtilab on Feb 1, 2012
Latest reply on Feb 6, 2012 by lhornburg
I am getting the Query UNTERMINATED error when trying to start a scan using the latest version of BenchLink Data Logger and a 34970A.

Communication has been established with the unit, and I was even able to upload a configuration from the 34970A.  Have tried this with two different laptops and get the same error.  One of the laptops is running Windows 7 Home Premium and the other is running Windows Vista Home Premium.

We are using a ProLogix GPIB-USB 6 converter for our communications interface.  The Agilent IO libraries are current.

I have uploaded a couple of screen shots for reference.

Thanks for your help.

David  

Outcomes