I have a 33521A with 16MB memory. I load two short data blocks into waveform memory. I then create a complex waveform using the DATA:SEQ command. I want to create a large number of sequence steps (2500 to 3000 steps). I get the following error: "873 Arb: Too many sequence steps". What is the maximum number of sequence steps?
According to the manual the max number of steps is 512.