AnsweredAssumed Answered

Downloading a Command Expert Command set for N5230C

Question asked by s.cohen on Jul 9, 2012
Latest reply on Jul 9, 2012 by hognala
Hello,
I'm new to the Agilent Command Expert. I'm trying to make  it work on a offline computer. The problem is that I don't have any command sets available. Moreover, I don't have a computer connected to the Internet with Command Expert installed.
Which means that I can't download the SCPI drivers using the program.
Is there any way to download the files directly without the program being installed?

Thanks,
S. Cohen

Edited by: S.Cohen on Jul 9, 2012 2:49 AM  

Outcomes